VM.STATE

Description

VM.STATE contains the state of the Virtual Machine. The following numeric values correspond to the following states.

  1. Valid program is currently being executed.
  2. There is no valid program in the drive.
  3. Valid program exists, not running now, but ready to go.
  4. Valid program has terminated.
  5. Program encountered run-time error.
  6. Program is invalid (e.g. bad CRC).

General Information

Type

R/O

Units

N/A

Range

0 to 5

Default Value

None

Data Type

Integer

Start Version

M_01-00-00-000

Variants Supported

This parameter is only supported on AKD BASIC drives.